May be a silly question - is it possible somehow to turn LTC4367 into LTC4367-1 without replacing component? We have already gotten a batch of boards but there is such a silly mismatch...
May be a silly question - is it possible somehow to turn LTC4367 into LTC4367-1 without replacing component? We have already gotten a batch of boards but there is such a silly mismatch...
Hi ADI expert
I have a application that needs two LTC4367 as an Or-ring but connects to the same power source
why I need to do this is not for current sharing but redundancy.
May I know if there is any side effect of the architecture?
I think the current…
Hi,
I am evaluating the over-voltage protection circuit and came across LTC4367. I wanted to know if I can use the same for a 40A motor load. I am trying to use it in between my buck and motor controller. My system is running on a battery?
Thanks a lot…
Dear Aaron,
wau, this is answer which I did not expect. Really nice and very helpful!
Thank You very much for Your effort, resistors, tips about oscillations, pullup resistor, etc.!
OK, below is almost "final schema":
- Added pin for Power Supply…
Hi Analog and Linear experts,
I used LTC4367 as a protection for power section of my board. as you see in attached image the circuit is like what said in datasheet. but it doesn't work even in normal range of voltage like 12V. in the output of this IC…
The datasheet for the LTC4367 list a number of external MOSFETS, however these are all relatively low power devices (max 4.5A).
Could you recommend any devices suitable for a larger load current?
Would IPD034N06N3GATMA1 be suitable for use (in a pair…
Hello
I have 2 questions for you
Is the LTC437 can be use as an ORING diode for multiple ( 3-4) power supplies . It seem that page 15 of the datasheet warn tha is not possible....why that ?
As an alternative solution i thought about LTC4359 but there…
Hi Analog and Linear experts,
I have problem with reverse supply protection, at LTC4367.
When I connect reversed supply to IN, at OUTput is measured negative voltage instead 0V.
All others LTC4367 functionality with positive supply work correctli (UV, OV…
Hello,
Im using LTC4367 as reverse polarity and load dump protection. My device get damaged when some load is applied (2A when testing).
Gate charge pump stopped working and Vgate=VIN, OV and UV dont work and device is always on when SHLD pin is 0V. I…
Hi!
I would like to use LTC4367 like the datasheet recommends.
Page 17 Figure 19
It is designed for 12V battery which should stop at 14.6V.
However, I want to design it for 24V which requires 30V Over Voltage.
The only thing I want to change is R1…