I am looking for a reference circuit for ltc4352 and Spice model. Although there is reference on the product page to the LTC4352, there is no link.
Thank you
I am looking for a reference circuit for ltc4352 and Spice model. Although there is reference on the product page to the LTC4352, there is no link.
Thank you
Hello,
Could you provide me with the ESD ratings for LTC4352? I could not find it in the datasheet.
Thanks in advance!
My LTC4352 often fails,Drive voltage is very low。Does the chip have high requirements for PCB wiring? Are there any common reasons for chip failure?
Hope you reply as soon as possible,Thank you!!
My Personal Mailbox addr: 308221147@qq.com
I am testing the LTC4352 to switch a MOSFET and I am changing the UV input pin to VCC and GND to turn it on and off, but the MOSFET stills quite the same. I have an LED as the load and it doesn't turn on and off when I change the voltage at the UV pin…
I have the LTC4352 component and 3 different qualifications appear in the datasheet.
Hi all,
I was wondering if LTC4353, that seems to be the doubled version of LTC4352, accept back-to-back connection for the external mosfet.
Is it possible?
The datasheet do not mention this possibility, but this is available in the little brother LTC4352…
Hello,
Is there a way to operate LTC4352 at higher voltage than 18V?
LTC4359 would be an option, but it is too slow for my application.
Thanks a lot.
Best regards
Hello,
I am looking for a fast switch On/Off Ideal Diode controller with back to back N-Mosfet like LTC4352, but with higher maximum input voltage (up to 24V).
Any clue, someone?
Thanks a lot.
Regards.
Hi, Yes, due to the MOSFET's internal body diode, Vin1 can never be completely cut off from output. It requires back-to-back FETs but LTC4353 doesn't work with back-to-back FETs. LTC4352 (single) works with back-to-back FETs. This is a prioritized supply…
Hi owp_ee,
We have the LTC4352 ideal diode controller , that can be used form 0-18 V , with an external supply. It controls external NFET and is available in 3mmX3mm DFN and 12-pin MSOP packages. LTC 4353 is dual gate version of this. Note that these are…