HI All,
can you tell is it possible to couple DC power to the LTC4331 twisted pair in order to supply the I2C slave ?
Best Regards,
D.
HI All,
can you tell is it possible to couple DC power to the LTC4331 twisted pair in order to supply the I2C slave ?
Best Regards,
D.
Hello,
The CTRL pin is described as controlling the remote from the local. What does the local control?
I'm using the local and the remote CTRL pins open. Is there any problem?
Regards,
Kazu
Hello there,
We are using the LTC4331 in our equipment, but randomly, our master receives NACK signals after sending a slave address. These slave addresses has been correctly acknowledged over few previous transactions, and the problem is manufacturer…
Hello
Is the I2C link rate limited by the SCL frequency?
I am thinking of setting the link rate to 500kHz or 1MHz with the SCL frequency = 400kHz.
Which link rate (500kHz or 1MHz) is better?
Regards,
Kazu
Hi,
I'm experimenting with the LTC4331 demo board, with my own uproc board. My setup is:
uproc <===> local LTC4331 <===> cable <===> remote LTC4331 <===> EEPROM
program is simple: continuously reading from (remote) EEPROM,…
No fix planned at this time. We will be either updating the datasheet or provide a separate errata document. The current workaround is to have your I2C driver perform a Remote Reset operation using the local ON pin in case the LTC4331 NAKs X number of…
Hello,
I've readed the datasheet of the LTC4331 and I'm in a case pretty similar to the one below:
I need sa solution like the central I2C slave but I would be more interested on having only one LTC4331.
I would like to know if it's possible…
What are the supply requirements for the LTC4331?
The new LTC4331 I2C Slave Device Extender looks like a great product. I would like to evaluate it in my system. Will there be a eval board available?
Thanks,
- Craig