• LTC4283 EEPROM WRITE

    Hi.

    I am writing to EE_CONTROL_1 (0xAA) and EE_CONTROL_2 (0xAB) in the LTC4283 EEPROM.
    If I write one byte at a time twice, it will match, but if I write two bytes in succession, it will fail.
    Is it not possible to write multiple consecutive bytes to EEPROM…

  • LTC4283 Faults/Alarms

    Hi.

    The LTC4283 writes a fault to the EEPROM fault register when an alert occurs, but it also writes to another volatile register.

    Should I read the EEPROM when ALERT # occurs? Should I read the volatile fault register?

    Also, are both the same value when…

  • LTC4283 FET_ON_STATUS and GATE_HIGH

    HI.

    Ask about FET_ON_STATUS and GATE_HIGH in the SYSTEM_STATUS register LTC4283.
    If FET_ON_STATUS = 1 and then GATE_HIGH = 0 for some reason, FET_ON_STATUS will also be 0. What is the difference between the two operations?
    Is it possible that FET_ON_STATUS…

  • RE: TC4283 I2c address

    Hi Zunda,

    Yes, only 8 LTC4283 can be connected to the same I2C bus. 

    Its configured with possible 8 different addresses using ADR0 and ADR1 pins mentioned in Table 1 of page 8 in the respective datasheet.

    If you want to connect more than 8 of the LTC4283…

  • RE: LTC7004IMSE#WTRPBF FIT data

    Hi ducdao,

    Apologies for late response. Please see this attached document:

     PDF