• LTC4267

    Hello everyone,

    I am in search of LTC4267 PSpice model  for my POE switch.

    Where can i get it?

  • RE: DC981A/B

    The input voltage range you specify falls below what is allowed for IEEE 802.3af compliance and is below the minimum LTC4263 V_SUPPLY.  Refer to the LTC4263 datasheet Electrical Characteristics for V_SUPPLY voltage range.  A PD interface controller for the…

  • LTC4367 1A load issue

    Hi,

    I am using LTC4267 IC as a over voltage protection device. I have set the over voltage to 36v and the device is working fine. I have given a load of 1A. I have given 28v supply and 100V supply using diodes ORing circuit such that

    1. If 28V is ON…

  • RE: LTC4367 problem

    Hi,

    I am using LTC4267 IC as a over voltage protection device. I have set the over voltage to 36v and the device is working fine. I have given a load of 1A. I have given 28v supply and 100V supply using diodes ORing circuit such that

    1. If 28V is ON…

  • Class 3

    A customer is submitting an order for a redesign of the ADI laser board. It looks like the documentation (The BRD file) calls for class 3 inspection, which apparently has significant financial overhead:

      

    If the plan is to use the board as a research device…

  • LTC6957-3

    Hi Team,

    We have using LTC6957-3 for Clipped sine to CMOS conversion, we using single output only, what we will do unused output PIN? 

    Thanks, Regard

    Anoop Varma m

  • RE: 3-Phase 4-wire in to 3-Phase 3 Wire

    Good Afternoon

    The ADE7878 can be configured to accept multiple different configurations including 3 phase 4 wire and 3 phase 3 wire wye and delta.  Our FAQ:  AN-639 that is available on our website has detailed diagrams of each connection on pages 12…

  • LTM2987 VOUT_EN[0..3]

    Good morning,
    I write for information on the pins VOUT_EN [0..3] of the LTM2987 power sequencer.

    Can the output of these 4 pins be changed via the LTPowerPlay tool? I need these 4 enable to generate 3.3V. The datasheet shows that…