• RE: Initial failed for LTC4266

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • LTC4266 detect function in auto mode ?

    Hi, all,

    good day!

    I meet a question, it is "how many detect function when LTC4266 work in auto mode ?" 

    My customer got some information of micro semi PD69204 from micro semi FAE..

    He says PD69104 has Current and power detection when IC…

  • RE: Serial Control Interface commands for LTC4266

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: PSE and Gigabit ethernet switch reference design

    And for the PSE, you could use an LTC4266C or LTC4266. See our DC1366B evaluation kit.

    Best Regards,

    Eric

  • RE: LTC4258 tICUT Fault issue

    The inrush appears to peak at 200mV, which is 400mA with the default 0.5Ohm sense resistor.  It is hard for me to interpret what the time/div of the zoomed in shot, but I can assume it is <<100ms/div.  So the inrush appears to be quick and should…

  • Q1: Cannot load COM Module

    If you receive a Cannot load COM module error message when trying to install a driver for a demo board using QuikEval, the following locations can be used to manually install the COM module. After downloading the module, run the installer and the software…

  • RE: Cannot load COM Module

    Hi Guy, 

    Thanks for this. I just copy paste the info here below to close this thread. 

    Part Number DC Board Number Class ID Url
    ADL5920 EvalADL5920 D5596 ltspice.analog.com/.../ins5596.msi
    LT3964 DC2424A D3964 ltspice.analog.com/.../ins3964.…
  • RE: LTC7004IMSE#WTRPBF FIT data

    Hi ducdao,

    Apologies for late response. Please see this attached document:

     PDF

  • LTC4266C backoff time test by sifos

    Hi ADIexpert

    my customer has issue for LTC4266C backoff time test by Sifos

    please see the quote from Sifos for Tdbo test

    The one PSE Conformance Test Suite parameter affected by ALT-B versus ALT-A power feeding is Tdbo (det_time test), the detection back…

  • RE: LTC4266A auto mode :The port is out of power and cannot be restored

    The LTC4266A at a high level is a Hot Swap controller that takes power from an isolated power supply and passes it over to the port output after safe detection of a valid PD.  It is not clear what you mean by "power supply".  Please provide further…