• RE: .file_attr 1="1";

    Hi Gideon,

    Sorry for the delay in responding.

    The cause of the problem is "-file-attr CORE0" and "-DCORE0" both being included on the compiler command-line. Could you delete CORE0 from the "Additional attributes" in Tools Settings > CrossCore Blackfin…

  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…

  • ADF7030-1

    Hello,

    I bought the ADF70301 - 433 EZKIT and I can't find, in the ADF70301 data sheet, the noise figure of the transceiver. 

    So I'm here to ask: how can i measure the noise figure of the ADF70301 using the 433EZKIT?

    Thank you for your support

  • ad7656-1

    I'm requesting the gerber files for this product mentioned above... is it possible to receive them. thanks, 

  • LTC2439-1

    Hi!

    We wanna use the LTC2439-1 configured with 16-Channel Single-Ended Inputs, the Reference-Voltage is 5.0V and the Input-Channel Voltages are from 0-5.0V

    But the datasheet does not clearly describe the function for us with this configuration.

    We are not…

  • AD7988 - 1

    Good afternoon....

    I currently am using the above subject successfully in a design.  The power supplies are as follows: Vref = 2.5V, VDD = 2.5V and VIO = 2.7V - 3.6V.  Moving forward I would like to re-route the analog supply, VDD to track with VIO.  Can…

  • ADUM4121-1

    Can ADUM4121-1 gate drive handle 100% duty cycle?

  • LTC6804-1 Automotive Grade??

    Is LTC6804-1 an automotive grade part i.e. AEC-Q qualified? What grade (0/1/2) is it? Thanks!

  • LTC3300-1 problem with communication

    Hi everybody,

    I have problem with SPI communication between STM32 and LTC3300-1. I have only one LTC3300 and only one LTC6810. No IsoSPI, no DaisyChain. The ICs have separated CS/SS signals. I want to manage 6S Li-Ion battery pack. The literature, I have…

  • ADA4945-1 MODE polarity

    Hello AD,

    Please clarify the MODE polarity of the ADA4945-1 in the datasheet.