• LTC4238 Bad FET Fault

    Hello,

    I am using the LTC4238 for driving 28V/22A load. Planning to use the LTC4238 (n-channel IPB044N15N5) in single driver configuration as shown in Figure 7 of the LTC4238 datasheet. My query is regarding the FET bad fault which has threshold of VDD…

  • LTC4238 QFN Pad Connection

    Hello,

    For the LTC4238 QFN device, please let us know if the exposed pad shall be connected to GND or left open.

    Regards

    Gaurav

  • LTC4238 reverse input protection

    Hello,

    Can the LTC4238 be protected against reverse input by adding a Schottky diode in series with its GND (and EPAD) pin? The max supply current in the datasheet is only 5 mA. Would this protect the LTC4238 from reverse input voltage of -45 Vdc, and…

  • LTC4238 22A Single MOSFET Design

    Hello,

    I am using the LTC4238 for driving 28V/22A load. Planning to use the LTC4238 (n-channel IPB044N15N5) in single driver configuration as shown in Figure 7 of the LTC4238 datasheet. My query is regarding the FET bad fault which has threshold of VDD…

  • LTC4238 100V Transient Operation and Reverse Supply Protection

    Hello,

    Can LTC4238 used for 56V nominal input power and 100V 100ms transient input voltage(MIL-STD-1275 surge voltage)?

    Absolute maximum values are 100V for LTC4238. But i am not sure can it be used for 100V 100ms transient input voltage.

    And can LTC4238…

  • RE: Limiting Inrush Current

    Hello,

    in principle any of our 24V capable HotSwap parts can do the job, more critical will be FET selection as you ask for a large SOA during startup.

    Our LTC4238 is tailored for such high power/high voltage apps. (Staged start with two current paths…

  • RE: Paralleling DCDC converters request

    Hi EngJunkie,

    Could you possibly let me know if analog devices has anything in this line : "This would also saves you of designing parallel converters (multiphase) that would warrant active sharing". Also how would this work?
  • ADI 全新中文资料(2021 年 5 月)