Is it possible to use the Gate pin of LTC4234 to drive an external NMOS in order to achieve reverse supply protection?
Is it possible to use the Gate pin of LTC4234 to drive an external NMOS in order to achieve reverse supply protection?
Hi team -
I am looking for 12V Hot swap solutions with below features .
I prefer to use integrated…
Hello,
We use an LTC4234 as hot-swap controller for a card powered at 5V DC nominal. The maximum current it can draw is in the order of 16A. The output load capacitance is 900uF in three groups of 300 uF (220uF polymer electrolytic + 8x10uF ceramic),…