请问:恒压输出的锂电池(每节1.5V),三节串联,能用LTC4150进行剩余电量的测量吗?
Hello,
I would like to know if you have other LTC4150 coulomb counter for batteries up to 12V, up to 15 V or up to 24V
I need a coulomb counter to sense 3 or 4 Li-Ion in serie and I don’t know what it is the best option.
Could you help me?
…Hello,
I am trying to design the LTC4150 into a NiMH battery powered product, but am confused as to whether it will work because I have 2 different operational modes. I have my normal run mode that draws around 100mA and my low power mode where the LTC4150…
Hi.
I'm using the LTC4150 on an embedded IOT design.
The design is running from a 7.2V Lithium Primary Cell (2 x 3.6V) , and the battery is not chargable, only discharge.
The LTC4150 has been connected between the 7.2V Supply and the device power…
手册的此处文字描述,这个“11%”,请问是如何计算的呢?谢谢!
LTC4150 Coulomb Counter: Device fails getting very hot when I use a 5 Ohm Current sense resistor ????
When I use a 0.05 Ohm sense resistor the LTC4150 works just fine.
Switch off & replace the 0.05 Ohm sense resistor with a 5 Ohm device (to give me…
Why is a RC filter recommended at the input of LTC4150 when it is not recommended for LTC2944 when they both have fairly similar structure?
Hi.
I'm really curious why you would like to amplify the inputs to LTC4150's sense pins. I think it would be simpler to just choose the proper Rsense value using equation 1 in page 8 of LTC4150's datasheet. Just input the maximum load or charge current…
Hello Siglo
Sorry about the delay! Many thanks for the attention on the question!
I uploaded the schematic. The demo board offered the PCB format files. So my layout just adds some functions to offered PCB layout file.