Hello everyone,
I am designing a solar powered device from a 22V (maximum) solar panel and a 3.7V 4000mAh (1S2P) battery, but the datasheet says nothing about the battery undervoltage lockout.
Does the LTC4091 have battery overdischarge protection? If…
I designed a circuit based on DC2558A development board, the problem is when battery voltage is higher than 3.6V, the LTC4091 seems not provide charging current.
Thanks for any help.
Siwakorn
Hello,
we designed a circuit based on LTC4091. The circuit is an almost identical clone of the DC2558A development board (that we do not have, by the way). The only difference is that the output current is set a little higher as well as frequency.
I…
Kindly suggest me a part similar to LTC4091 which can act as backup switch and charging LI-Ion 7.4v Battery
Hot 100 是 EDN 一项承传已久的历史活动,每年美国的编辑们都会选出当年最热门的100款产品分享给大家。
2017 年最热的产品有哪些?EDN 编辑根据自己的判断和读者的兴趣选出了100个热门产品,其中 ADI 有 16 款产品上榜!手动鼓掌
登上 EDN Hot 100 的 ADI 十六款产品都是哪些?它们为何如此受青睐呢,版主今天为你们说道说道~
模拟器件:
LTC2358-18 是一款 18 位、低噪声、8 通道同时采样逐次逼近型寄存器…