• RE: LTC4015 can charge VBAT from 1.8V to 2.8V ?

    Hi Hiroyuki,

    LTC4015 cannot charge at such low voltages. Perhaps take a look at LTC4012:

    https://www.analog.com/media/en/technical-documentation/data-sheets/4012fa.pdf

    Regards,

    Zack

  • LTC6957-3

    Hi Team,

    We have using LTC6957-3 for Clipped sine to CMOS conversion, we using single output only, what we will do unused output PIN? 

    Thanks, Regard

    Anoop Varma m

  • RE: 3-Phase 4-wire in to 3-Phase 3 Wire

    Good Afternoon

    The ADE7878 can be configured to accept multiple different configurations including 3 phase 4 wire and 3 phase 3 wire wye and delta.  Our FAQ:  AN-639 that is available on our website has detailed diagrams of each connection on pages 12…

  • AD5421 in 3-wire circuit

    I have an existing circuit using the AD5421 as a 2-wire loop-powered transmitter.  It has a CPU, LCD display, sensor ADC, and an AD5700 for Hart transmission.  Works great.

    My customer wants to add additional circuitry that would only be used if the device…

  • ADE7880 - 3 phase 3 wire delta configuration

    Hi,

    As per the ADE7880 datasheet pg. 43, in three phase three wire delta configuration, Phase B active, reactive and apparent powers are 0.

    So, I would like to know if there is a way to find out the Phase B power data in three wire delta configuration…

  • ADUC843BCPZ32-3

    你好,

    咨询下单片机ADUC843BCPZ32-3 的技术问题:

    1.)参照DATASHEET, PSEN脚在代码执行模式下应该输出高,实际输出为低(0.005V左右)。

    2.)PSEN脚最大允许输入电压电流各为多少?

    3.) 代码运行过程中,PSEN管脚可否通过电阻上拉到电源?

    请给与大力支持!

    谢谢!

  • ADF4355-3

    In ADF4355-3  frequency synthesizer , 

    can  i use both RF outputs A and B at the same time ? 

    because iam using this IC to generate LO for two channels at the same time .

    what is the Rf output level of the both A and B at 4 GHz ? 

  • LTM2881IV-3

    1. When the thermal shutdown function is activated at 125, can the IC be back to its normal working condition when the temperature drops to some degree?
    2. For the over current protection function, will it shut down the IC? If yes, what is the maximum current…
  • ltm2881-3

    该芯片 没有5V输出,隔离前端输入正常,ON使能也拉高,但没有5v的输出.