• Inquire of cell# limitation of LTC4010

    Hello,

    We plan to apply a 24V battery using 20 cells of 1.2V Ni-cd battery.

    It is confirmed that 1 to 16 cells are supported on the LTC4010 Datasheet.

    Please check if it is possible to use 20 cells and If you have any considerations for use, please ask…

  • LTC4010

    LTC4010 for NiMH battery charger application. There are some field failures: CHRG indicators ON, FAULT off, no PWW, no charger current. VTEM 10k to GND. 

  • RE: LTC4010 eval board or reference schematics with BOM

    Hi Fausto,

    Take a look at the LTC4011 demo board: https://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/dc674b.html

    There is a schematic/BOM in the demo manual.

    LTC4011 is nearly identical to LTC4010 but it has…

  • RE: LTC4162 for NiMH batteries

    Hi Dmitry,

    No, unfortunately. I would recommend LTC4010 or LTC4011 for such a design.

    Regards,

    Zack

  • RE: NiMH - LTC4015 battery charger

    Hello,

    I might recommend LTC4011 for your application. This is a NiMH charger with proper termination functions (which I recommend for charging at 1.5A). It is a buck charger without a boost feature, so you will need to follow it with a boost converter…

  • LTC4011:About the body diode of the external FET

    Hi, I would like to use LTC4011.

    So, I have a question. Please help me.

    Question:

    I am experimenting with the LTC4011.

    I'm writing a circuit diagram first.
    When checking the reference circuit, there is an unknown point…

  • LT4010 tgate switching issue

    In my circuit, after power on, /CHRG LED was blinking (0.1sec on in every 1 sec) during the first 10 second , /CHRG LED was ON during the next 2 second

    and finally /FAULT was detected.

    I attached vcc,tgate waveform I monitored.

    just before /FAULT was detected…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032