• LTC3722 & LTC3901 : Synchronous rectification not working correctly

    Hi,
    I am planning to design a 2.5kW (84V 30A) PSFB converter (offline with Vin = 390V) for a battery charging solution. I have somewhat understood the ways by which this topology achieves ZVS and the significance of Leakage/shim inductance, Mosfet Coss…

  • LTC3723-1 and LTC3901 synchronous push-pull: LTC3901 SYNC pin not working correctly in LTspice

    Dear Power by Linear,

         I wanted to attach the actual .asc file, but the forum insert function keeps giving me an error. So, an image of the circuit is below.

    All of the example circuits and evalboards I could find use a gate drive xfmr whose datasheet…

  • LTC3901的Rcsx1,Rcsx2,Rcsx3的取值问题

    在读取芯片LTC3901的时候, ,里面所指示的Iripple代表的什么时候的峰值电流?比如我参考典型电路https://www.analog.com/media/en/dsp-documentation/evaluation-kit-manuals/DC719.pdf,但是输入电压是18-36V,我的变压器匝比是3(初级):3(次级):3(次级),输出电感用6.8uH其他参数不变,我该怎么取值R50,R51,R21?期待您的回复,谢谢

  • RE: Enquiry for part LT3091HDE#PBF (SO# 813674)

    Hello glyeo, 

    Material purchased from authorized distribution are genuine. ADI cannot comment on material purchased from unauthorized sources.  (Sales and Distribution | Analog Devices ).  

    PCN's are listed on the Sample and Buy section of the product page…

  • RE: Can the full-bridge be paralleled?

    Hi

    I would recommend the LTC3722 with the LTC3901, and yes, the converters can be paralleled. I would use an ideal diode on the output of each converter to prevent negative current issues, the LT8672 would serve. Here is a general circuit that can be adapted…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032