• LTC3891 -PLL Input

    Has anyone used the PLLIN/MODE for external synchronization?

    I've tried all the options shown on the evaluation board schematic and had no luck.

    Other circuits that I've designed recently using the LTC3895 and LTC3858-1, have both worked as described…

  • LTC3891输出开关频率只有设定值的1/10

    最近在使用LTC3891做DC-DC时,遇到这个问题:在进行开关频率调节的时候,根据数据手册所给的要求,对FREQ引脚的下拉电阻进行不同值的调试;同时Mode也进行了分别接到GND和INTVCC两种状态去调试,发现TG和BG上的频率与数据手册所给的频率图表对不上,每一值都相差10倍左右,测试时是将MOS断开进行测试的,请问是什么原因导致这种情况?什么方法可以解决这个问题呢?谢谢!  XLS

  • LTC3891 - Over-temperature Protection?

    Hi,

    We use the LTC3891 controller in our buck design, 24V to 5V, 1.4W.

    We have performed some thermal characterization tests on our design up to 175°C and maybe more, depending on oven calibration (less than 200°C).

    The 5V buck has been turned…

  • LTC3891 PLLIN

    Sorry, repeat question that I asked in the wrong forum.

    Has anyone used the PLLIN/MODE for external synchronization?

    I've tried all the options shown on the evaluation board schematic and had no luck.

    Other circuits that I've designed recently using…

  • RE: LTC3891 - maximum voltage adjustment range ?

    Hello,

    the limitation towards 24V comes from the current sense opamp inside the LTC3891. The SENSE+ and SENSE-  pins have an absmax rating of 28V. So if you go beyond 24V internal opamps will not work properly AND (more severe) is a possible failure reason…

  • LTC3891 low output current

    I cannot reach the design current of 6A with this IC.

    The maximum current I can achieve is ~1A, if I increase the load further the gate drive signals clash. I have experimented with adding additional capacitors in the input, output and after the output…

  • RE: 请教一下关于LTC3891开关电源遇到的开关频率调节问题

    最近I在应用LTC3891的时候,也遇到了同样的问题,mode设置为突发、强制连续模式,都是输出频率只有设置频率的1/10,请问是什么原因导致的呢?该怎么解决呢?!不胜感激!

  • LTC3891 support 12V/20A

    Hello

                Could LTC3891 support 54VIN to 12V/20A (non-isolate) ? What is max OCP of LTC3891? Thank you.

    BR

    Patrick 

  • LTC3891 RUN pin noise

    I am currently utilizing the LTC3891 with a 499k between PWR and RUN and a 100k between RUN and GND.  I do not need the UVLO function, and I believe I am potentially picking up noise on this device that is causing the RUN pin to go low.

    The LTC3891 says…

  • It’s Always the Electrolytics

    A friend asked me a few years ago: “You are an electronics engineer aren’t you?” Somewhat hesitant to reply, I answered that I was. This is normally greeted with questions such as: “Can you fix my PC?” or “Can you unlock my mobile phone that the FBI…