• RE: parallel LT8930A controller clock synchronization without external clock?

    Can clarify the ADI part number, there is no LT8930 product. Do you mean LT8390 or LTC3890?

  • ADF4355-3

    In ADF4355-3  frequency synthesizer , 

    can  i use both RF outputs A and B at the same time ? 

    because iam using this IC to generate LO for two channels at the same time .

    what is the Rf output level of the both A and B at 4 GHz ? 

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • RE: 3-Phase 4-wire in to 3-Phase 3 Wire

    Good Afternoon

    The ADE7878 can be configured to accept multiple different configurations including 3 phase 4 wire and 3 phase 3 wire wye and delta.  Our FAQ:  AN-639 that is available on our website has detailed diagrams of each connection on pages 12…

  • ada4411-3 don't work

    AD技术支持您好:

    我遇到一个比较棘手的问题,我使用的ADA4411-3芯片不工作;我使用的ADA4411-3器件手册上的参考原理图设计的,ADV7340芯片输出RGB视频信号给ADA4411-3进行滤波,但是ADA4411-3有输入信号无输出信号。

    如下图为ADV7340的RGB信号输出,并联300欧姆电阻到gnd。

    如下图为ADA4411-3的原理图,23管脚增益为4倍,1,24管脚幅度为600mV;15脚选择通道1,8,9管脚设置滤波通道00:36MHz;通道2无输入接下拉到gnd…

  • RE: AD9375 3-WIRE SPI

    Hi,

    I made the required changes for 3-wire SPI, to the original design, I pushed a new branch with this example.

    I was able to read and write from the AD9371 and AD9258.

    Please wait...
    WARNING: AD9528_initialize() issues. Possible cause: REF_CLK not connected…

  • ADE7880 - 3 phase 3 wire delta configuration

    Hi,

    As per the ADE7880 datasheet pg. 43, in three phase three wire delta configuration, Phase B active, reactive and apparent powers are 0.

    So, I would like to know if there is a way to find out the Phase B power data in three wire delta configuration…

  • LTM2881IV-3

    1. When the thermal shutdown function is activated at 125, can the IC be back to its normal working condition when the temperature drops to some degree?
    2. For the over current protection function, will it shut down the IC? If yes, what is the maximum current…
  • ltm2881-3

    该芯片 没有5V输出,隔离前端输入正常,ON使能也拉高,但没有5v的输出.

  • ada4412-3

    Hi,

    I want to know  :

    1. what is the minimum, typical and maximum supply voltage recommended for ADA4412-3.

    2. What is the supply current to measure power dissipation?

    3. Analog supply voltage or digital supply voltage (It is not clear in the datasheet…