• LTC3890 Demo Board DC2236A modification not working

    Using the DC2236A board as reference, I narrowed the input voltage using the same LTC3890 part from 14V < VIN < 18V but run at a higher frequency of about 400Khz at max current 18A.

    using the available LTpowerCAD, I obtained those adjusted values…

  • LTC4000 & LTC3890 and the ITH pin

    I have connected LTC4000 with LTC3890 to create a UPS  with a Li-ion battery pack. I have problem that the pin ITH has always the value 0.4V. As a result the voltage out the converter (LTC3890) drops from installed value 21.3 to 16.1V. Also the converter…

  • RE: LTC3890 & LTC4000 ITH pin connection

    That's great to hear Ayham! 

    Regards,

  • RE: Inquiry regarding Antislope Compensation

    Hi

    The designer has to make choices as to what features can be incorporated on a certain size die with a given process and meet packaging and cost constraints. Antislope Compensation was not given priority over other requirements on LT3845 and LTC3890…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • RE: ADP1031

    Hi Mehmet,

    I'm afraid the ADP1031 is not capable of providing such output power.

    Do you need isolation for your application? If not, ADI have bunch of Buck controllers that I think can cater your requirement (non-isolated) like the LTC3890 or the LTC3892…

  • RE: parallel LT8930A controller clock synchronization without external clock?

    Can clarify the ADI part number, there is no LT8930 product. Do you mean LT8390 or LTC3890?

  • DC2236A-B

    Hey All,

    I am working on de DC2236A-B and i adjust it so its output voltage turn to be 22V. As a results was the chip LTC3890 three time broken. I replaced it but i am not sure any more if this board will give the needed voltage. The only thing I have…

  • PWM solution proposed

    Master,

    Looking advise on ADI proposal. 

    I'm thinking of LTC3890 for Load B (18-24Vdc, Current 5-10A) 
    1. Isolated DCDC Converter, Input rated 24Vdc,300W; Output Voltage 18-24Vdc, Current 5-10A                                                                                  
    2. PWM Controller Module/Circuit, Input rated 24Vdc,30…

  • RE: Question about LTC7851

    Hello,

     

    The current sense inputs of the LTC7851 will need to be divided down to keep the voltage under their maximum rating. This may require precision resistors with a tolerance of 0.1% or better to minimize the common mode error due to resistor mis…