• RE: wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

    Hello,

    sometimes page one of the datasheet contains the answer:

    The LT8708-1 always operates as a slave to the master LT8708 and has the capability of delivering as much cur-rent or power as the master.

    Hence I would state, that LT8708-1 can NOT work…

  • RE: adum4121-1 voltage

    Hi Mehdi,

    which voltage exactly do you mean?

    Vdd1 can have 5V, and min input voltage (VIH) for signal inputs can be >0.7 x Vdd1. 

  • ADMV1014 Enable0/1

    Can the Enable (0 and 1) be left open or they have to be necessarily tied to 3.3 V ?

    Best regards.

    Maurizio

  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…

  • Powerful Combinations are Possible when 1+1>2

    It’s a new beginning for Analog Devices and Linear Technology. Together we become the high-performance analog industry leader with an innovation engine fueled by our comprehensive portfolio of analog and mixed signal products and solutions.

    We have…

  • About EVAL-AD7768-1

    hi

    when i use EVal-AD7768-1, can i connect the Ain+ and Ain- together to test the noise of the ADC? would you pls tell me how to test the noise of the EVAL board? thanks!

  • AD4110-1 Communication issue using development board EVAL-AD4110-1

    Hello all,

    I am facing issue in communicating with AD4110-1 via SPI pins in J2 connector on evaluation board using an external microcontroller. I am trying to read ID register as that register will be a static register hence it will be easy to know if…

  • LTC2955-1 auto-turn-on disabled with 1 second VIN removal

    I have a circuit which allows for auto-turn-on with battery application. (SET = VIN, ON = VIN, PB floating, KILL_N = high.)

    It appears that I'm running into a problem with the datasheet statement "after the EN output goes low, the LTC2955-1 starts the…

  • What the difference between the ADA4940-1 and the ADA4941-1?

    What is the difference between the ADA4940-1 and the ADA4941-1? They are both ADC drivers, but what distinguishes the two parts from each other?

  • RE: Can LT8708EUHG-1 be used as a standalone DC-DC?Can LT8708EUHG-1 be used as a standalone DC-DC?

    Hi Clark,

    Let's move this to the Power section so they can further assist you.

    Regards,

    Andrei