• About LTC3882 external DrMOS

    Hello

    I have a question about the LTC3882's external DrMOS.


    Is there a recommended DrMOS with the following specifications?
    Please let me know if there are any recommended products other than FDMF5820DC and FDMF6820A.

    Input voltage: 12.0V
    Output voltage…

  • LTC3882-1 issue

    Hello,

    I ran into an issue using LTC3882-1 in our custom design. We are using LTC3882-1 together with UCD7242 to generate 1.0V core Vdd for LS1046A processor. Only channel 0 of LTC3882-1 is used, channel 1 was set to be off. I am trying to figure out…

  • Questions Regarding LTC3882 Output Voltage Settings

    Hello

    I have a question about the output voltage setting of the LTC3882.

    I think the voltage of Voutn_CFG can be adjusted by an external resistor.

    A list of output voltages with external resistance values is given in Table 8 of the data sheet P59.

    Please…

  • LTC3882-1 ltp3 file request

    Dear, 

    Happy New Year~

    I was designed LTC3882-1 power.  it is used  70A power in memory tester. 

    No load operation was confirmed for the normal operation, But 0.1A load case, the ripple was measure peak to peak ripple 1V. 

    so, I want check LTpowerCAD libray…

  • LTC3882 CKT CONFIGURATION FOR 2-PHASE USE

     DOCX

    Hi,

    I'm planning to LTC3882 for generating 1.05V with 2-phase operation and request to confirm ckt (uploaded) is fine.

    Thanks in advance.

  • RE: Demo board DC2174A-A cannot configured output voltage.

    The bit 6 of MFR_CONFIG_ALL_LTC3882 is set to 0 by default (meaning that the LTC3882 will respect the resistor configuration). So if you put a default LTC3882 on your product (or make sure bit 6 of MFR_CONFIG_ALL_LTC3882 is set to 0), yes you can use resistor…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • 工程师必看丨一份来自ADI工程师的Power技术问题指南!

    作为电子电路的基本构成,电源可以说无处不在,通信、汽车、消费类电子……

    当今时代,电源广泛应用于各种热门的市场应用之中,并成为其必不可缺的一个重要组成部分。

    作为工程师,在电路设计中不可避免的会遇到电源技术的难题

    今天,斑竹为各位小伙伴带来了ADI工程师亲自盘点的ADI Power的技术问题集,希望能够帮到大家哦~

     PDF