• LTC3855 Differential Amplifier

    Hi,

    Using LTC3855, I am going to design one channel to output 1V and the other to output 6.3V.

    In order to use a differential amplifier, the Vout range must be 0.6V to 3.3V, and the data sheet states that it can output 0.6V to 12.5V when not in use.…

  • LTC3855 switching frequency

    Hello


    Our customer asks below about switching frequency of LTC3855.
    Please let me know your advice.

    Question
    When he measures TG2 of LTC3855 at 500KHz switching frequenct setting (FREQ=120Kohm) using his circuit board,
    its frequency is 250Khz. Then the…

  • LTC3855 5V in and 5V out

    Can LTC3855 realize 5V in 5V out?

    We have one situation, which is 5V in, or 12V in. No matter which one, we hope that the output is 5V.

    If 12V in, LTC3855 can buck the 12V into 5V, that is no problem.

    Here is the queation, if 5V in, Can LTC3855 shut down…

  • RE: The meanings of some parameters of chips and the interleaving ability

    Hello,

    The LTC3855 is a current mode controller. As with other current mode controllers the output voltage of the LTC3855 is limited by the maximum rating of the SENSE+/- pins with respect to ground. These pins sense the voltage across the sense resistor…

  • RE: LTC3892-1 Eval Board

    Hello Hiro-San,

    I do not know the reason why R17/R18 differ from R19/20 in the eval-Kit. As you stated other documents (LTC3855) show here two identical values (LTC3833 as well).

    My rough guess would be that this setup perform slightly better for the…

  • DCR Sensing

    Hi,

    I would like to know is there any difference on the placement of the Inductor DCR sensing.

    On the datasheet of LTC3784 the DCR sensing the capacitor and resistor is parallel, whereas on the application note 136 using LTC3855 the application note…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032