Referring Data sheet 3810fc for LTC3810 I can not find the specification of dead time between main output FET operations. So how does one determine the largest gate charge that can be switched quickly enough?
Referring Data sheet 3810fc for LTC3810 I can not find the specification of dead time between main output FET operations. So how does one determine the largest gate charge that can be switched quickly enough?
hi guys,
how i have to design the ltc3810 circuit layout to get a constant current limited output?
1. we use a precast pcb product design
2. we configurated the output voltage over the Vfb Voltage divider to 29,28V output CV
3. we try to limit the output…
hi guys,
how i have to design the ltc3810 circuit layout to get a constant current limited output?
1. we use a precast pcb product design
2. we configurated the output voltage over the Vfb Voltage divider to 29,28V output CV
3. we try to limit the output…
1. the schematic of the application
Vin=84V, Vout=50V,fsw=1.04MHz,full load current is 2A.
control section: LTC3810
driver section:LMG1210
Switch transistor: high side:EPC 2012C low side: EPC 2012C
2. The problem we were faced with in the experiment…
Hello,
Engineers Forum,
Analog Devices.
I am a Senior Electronic Designer from Simyog Technology Pvt.Ltd, a start-up from Bangalore, India and funded by Robert Bosch, India. In one of our applications for Automotive electronics, We would like…
24Vout@10A的方案都得需要外置的MOSFET,所以可以参考LTC3895/LTC7801/LTC3810/LTC3703。如果输入电压有可能低于24V的话,可以看一下LTC3779,LT8705A。
I am designing a circuit using the LTC3895.
Why is not the provision of "BG, TG RMS Currents" in LTC3895?
For example, the LTC3810 has the following.
<---
FET is thinking of IPP50N10S3L-16 (infineon).
Qg (Gate charge total) is 64nC, is this…
各位筒子们,又到了这个月的热门问答帖时间~
这次,为大家带来的是来自咱们中文论坛的ADI Power系列问答20则!这些问答都由ADI工程师精心解答,绝对干货满满~
好啦,话不多说,咱们开始吧
问题一、LTC4162-L42充电功能异常应该如何解决?
问题二、LTC3891IFE调整电阻使输出电压为5V,输出电流可以达到多少?
ez.analog.com/.../ltc3891ife-5v
问题三、LTC3026的SW管脚应该悬空还是接地…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |