• LTC3785-1 PGOOD

    Hi,

    I am in the process of upgrading my LTC3785 design to use the LTC3785-1 variant so that I can take advantage of the PGOOD signal. 

    Can you please confirm if the maximum voltage of this pin is 6V.  This seems a little low for an Open Drain connection…

  • LTC3785 Burst Mode

    Hi,

    I have designed a 5V@4A boost-buck voltage regulator using the LTC3785 - I found the Excel Spreadsheet calculator tool and Applications Information provided in the datasheet to be most helpful in this process, thank you.

    However, I am seeing some…

  • LTC3785 Low Voltage Operation

    Hi,

    I am developing an application with the LTC3785 that will use a single Lithium Cell as the power source (3V to 4.1V). 

    The LTC3785 has an onboard LDO regulator (4.35V) that provides power for the FET Gate Drive signals.  The Block Digram in the Datasheet…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • 请问ADIS16495-1和ADIS16505-1,如何直接连接windows 10 pc使用呢。

    ADI工程师,

    1、我们开发的系统是运行在windows平台下的,现在需要添加IMU单元,请问这个能怎么通过USB连接PC或以太网口直接获取imu传感器的数据呢?

    2、请问你们的有相应的开发SDK吗?

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • ADA4700-1供电

    ADA4700-1手册写的是双电源供电,能单电源供电吗

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • LTM4644-1 LT POWER CAD 3+1 MODEL,

    CAN YOU POINT ME TO THE POWER CAD MODEL FOR 3+1, I ALREADY HAVE THE 2+2 AND 4.

    I WANT TO MAKE SURE I GET THE COMPENSATION VALUES CORRECT BEFORE BUILD.