• Using the LTC3785 with higher input voltage

    We've currently designed 2 power supplies using the LTC3785 that works off a input supply of 5 - 8.2V and outputs 5V and another that outputs 3.3V.

    Unfortunately the input voltage range has changed to 5 - 20V, this pushes it outside the spec of the…

  • LTC3785-1 PGOOD

    Hi,

    I am in the process of upgrading my LTC3785 design to use the LTC3785-1 variant so that I can take advantage of the PGOOD signal. 

    Can you please confirm if the maximum voltage of this pin is 6V.  This seems a little low for an Open Drain connection…

  • LTC3785 Burst Mode

    Hi,

    I have designed a 5V@4A boost-buck voltage regulator using the LTC3785 - I found the Excel Spreadsheet calculator tool and Applications Information provided in the datasheet to be most helpful in this process, thank you.

    However, I am seeing some…

  • LTC3785 Low Voltage Operation

    Hi,

    I am developing an application with the LTC3785 that will use a single Lithium Cell as the power source (3V to 4.1V). 

    The LTC3785 has an onboard LDO regulator (4.35V) that provides power for the FET Gate Drive signals.  The Block Digram in the Datasheet…

  • LTC3872 question

    Hi, I have a question about LTC3872: The carrying load ability for the output of the LTC3872 circuit is not good, I do not know what is wrong with my LTC3872 circuit configuration? can ADI engineer help me? And I will be very grateful!!!

    1circuit co…

  • LTC3872 circuit configuration

     PDF

    Hi, I have a question about LTC3872: The carrying load ability for the output of the LTC3872 circuit is not good, I do not know what is wrong with my LTC3872 circuit configuration? can ADI engineer help me? And I will be very grateful!!!

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032