Hi Yifeng,
Sorry for late reply. LTC3780 is a very popular part and we have no plans to obsolete it any time in the foreseeable future. We also expect it will still be available 8-10 years from now. Thanks!
Hi Yifeng,
Sorry for late reply. LTC3780 is a very popular part and we have no plans to obsolete it any time in the foreseeable future. We also expect it will still be available 8-10 years from now. Thanks!
Hello! I make a charger for assembling 6S using LTC3780 and MCU STM32. To change the output voltage of the LTC3780, I use a digital rheostat AD5174. Part of the circuit with LTC3780 and AD5174 attached. In this form, this circuit does not work: the output…
I'm using a LTC3780 as a buck/boost 5V regulator. I'm having some problems with the regulator doing some odd things if the input voltage is above approx 18V and the load on the device is increased
The images show the high side FET drive (blue…
Hi,
I am trying to utilize LTC3780 as a current source for the LED (2V x 5A). Unfortunately, at the startup I see a huge voltage and current spike (attached), which blows up the LED instantly. Is there any way to adjust slow startup (SS pin) feature to…
Hello,
Could someone be so kind as to explain how the RC filter is derived for the Ith Pin? One example shows an 8k and 2200pF, and another example has a 15k and a 10nF. Then a third example has a 68k and 3300pf. The datasheet explains it is a current…
电路参考淘宝买的一个Ltc3780模块,可以实现恒流控制,是这么实现恒流控制的:
输出回路上有个电流采样电阻,这个电阻两端的电压,经过运放放大后,再经过一个二极管,连接到Ltc3780的6脚VOSENSE+这个管脚,这个管脚的电压一旦超过0.86V,则会引起Ltc3780的输出过压保护功能,从而实现输出恒流控制。
经测试,输出接纯阻性负载时,可以实现恒流输出,虽然不太稳。但基本满足要求。
但输出接锂电池时,则恒流功能就失效了,无论输入还是输出电流很大。我量了下6脚电压,已经是3V多了。
Hi Yogesh
Please download LTpowerCAD and LTpowerCAD file for LT3780. After downloading the files, run the program and input your parameters to get the suggested ref design and parts.
http://www.analog.com/en/products/ltc3780.html#product-tools
One of 4 mosfets always opened in BUCK, other in BOOST. You may use Buck-Boost controller with external mosfets like LTC3780 to control it state. Also you may compare input and output voltage: if Vin>Vout - Buck else - Boost.
Good day.
My project uses Vin 9 ... 28 V. Lead acid battery 6 cells .. Charge current 5 A. Load current 10A.
I am faced with the problem of strong heating of the coil with a load of more than 3 A, the coil heats up> 70 degrees. The coil used is such a SRP1770C…