• ADA4310-1, 4311-1 with sloped PD0, PD1

    When using 4310-1 or 4311-1, with PD0 and PD1 pins taking values between 0V and whatever is considered logic high, does the amplifier behave reasonably? By that does it behave without going unstable or draining excessive current or requiring excessive…

  • 1:1 Baluns covering wide frequencies seem widely available. However, 1:2 Baluns seem to be narrower and less available. Why is this?

    1:1 Baluns covering wide frequencies seem widely available. However, 1:2 Baluns seem to be narrower and less available. Why is this? asked by Robert B.

  • AD8195:  1:1 HDMI/DVI Buffer with Equalization

    Is there any documentation for the evaluation board for the AD8195?

    Thanks,
    John

  • Differential video transmission with ADA4433-1 and ADA4830-1

    Hello,


    Thanks for providing the spice model of both ADA4433-1 and the ADA4830(-1).

    I'm trying to design a DC coupled differential transmission system using the ADA4433-1 and the ADA4830.

    The overall gain from input (ADA4433-1) to output (ADA4830…

  • LTC5588-1 and LTC5586 IBIS model

    Hi Experts:

    Could you share LTC5588-1 and LTC5586 IBIS model for simulation, thanks!

  • LTM8055 and LTM8055-1

    Dear Team,

    We are using LTM8055IY#PBF in our production.

    Since lead time of this item is high, for the same design we plan to purchase LTM8055IY-1#PBF as a drop in replacement whose stock is available.

    The only difference that I understand between LTM8055IY#PBF…

  • How to configure 1 TX-1 RX in No-OS

    Hi all,

        My design uses ADFMCOMMS2 module and ZEDBOARD, I want to transmit data using 1 TX- 1 RX but the default set 2  TX-2RX in No-OS, so what parameters in  default_init_param in main.c file I need to modify in order to  set 1 TX- 1 RX, thank you for…

  • Communication Issue between LTC6811-1 and LTC3300-1 via SPI

    Dear Colleagues from ADI,

    I've frustrated by this communication failure for quite long time, help from you is appreciated.

    SPI from LTC6811-1 can send out waveforms correctly and the code is as follow, but all two LTC3300-1 has no response(can’t…

  • (ADA4433-1) To connect ADA4433-1 to ADI Video decodor

    Hi !

    I have some questions about ADA4433-1.

    ******************************************************************************************

    Q1)

    Our customer are planing to make evaluation board to change "single-CVBS" to "Diff-CVBS" to input ADV7281A-M…

  • (ADV7390/1)Does ADV7390/1 supports ED-SDR 8bits 54MHz?

    Hi!

    I have some questions about ADV739*.

    (1)=========================================================

    I want to input BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit) to ADV739*.

    Does ADV7390/1 support that Video-format?

    Or must I use ADV7392/3?

    At the…