Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:
[Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
.file_attr 1="1";
syntax error is at or near text '1'.…
Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:
[Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
.file_attr 1="1";
syntax error is at or near text '1'.…
Greetings!
I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…
|
Hello,
In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?
Best Regards,
Hello Team.
1:1 transformer applied in IF pin is expensive.
so we want to use without transformer.
is it possible that?
Can you support solutions?
thanks.
Best regards,
Josh
I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…
Hi,
ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?
Regards,
Ivan.
Dears,
Does ADI have the solution that support 2 CVBS and 1 LVDS(5 wires) input then 1 LVDS output?
The CVBS signal is from camera and the LVDS is from video or navigation.
The output LVDS will display in 800x480/1024x600 screen.
This is the siganal…