• Absolute maximum voltage of Boost-SW of LTC3633A-2

    Hi,

    Is it correct that is absolute maximum voltage of Boost-SW voltage.
    I confirmed INTVcc voltage that is between 3.1V to 3.5V on datasheet. I also confirmed nearly 3.6V at Boost-SW voltage on board .
    It may think that reason of capacitor between Boost…

  • LTC3633A/LTC3633A-1 datasheet spec conflict

    Hi , 

    In the DS of LTC3633A/LTC3633A table on page 3 declares the value of VIN1 to be in the range of 3V to 20V , whereas the figure on page1 under "Typical applications" declares it in the range 6V to 20V . Which one is correct ?

       

  • LTC3633A-1 Efficiency

    The datasheet doesn't show much on higher output voltages. I am using an input voltage on 12V and an output of 8.5V at 2.7A on SW2 and an output of 5.5V at 2.7A. I wants see the efficiency  curve on it but didn't see any information on it or recommended…

  • LTC3633A output regulation problem

    I'm working with an existing circuit design that has successfully used an LTC3633A dual switching converter for the last 3+ years.  Our most recent board build is having problems with one of the converter outputs, and I'm having trouble identifying…

  • 关于在LT4363-2及LTC4364-2中的Retry Duty Cycle问题?

    敬启者,您好:

    在选择使用LT4363-2及LTC4364-2中有一个参数Retry Duty Cycle;

    关于Retry Duty Cycle,我的理解是:

    假定T1为Cctmr电容开始充电到MOS管关闭所需时间,Tcool为冷却时间;

    Retry Duty Cycle=T1/(T1+Tcool) * 100%

    LT4363-2:Less Than 1% Retry Duty Cycle During Faults, LT4363-2;

    LTC4364-2:0.1% Retry Duty Cycle…

  • Pluto - 2 Rx and 2 Tx using MATLAB

    Hi,

    I would like to setup the SDR Pluto to operate in 2 Tx and 2 Rx mode.

    I have followed the steps in the following video : https://www.youtube.com/watch?v=ph0Kv4SgSuI

    However, I am unsure how to setup and control the 2nd transmitter or receiver. 

  • LTC3633A output coupling switching noise

    Hi all,

    Our customer will be going to select power IC, mult ch output.
    They will be concerned the output coupling, and switching noise.

    In the datasheet LTC3633A, page 12 "OPERATION" say following.
    "One potential disadvantage to this configuration…

  • RE: ADA4940-2, issue on creating 2 differential signals around 0V

    Hi, 

    With a bit late, thanks for this suggestion.

    By applying -0.2V to R3, this circuits can convert 0 to 0.4V to a balanced -0.2 to 0.2V .

    It has been checked on the eval board.

  • ADV7611 YCbCr 4:2:2 SDR issue

    I am trying to configure ADV7611 to output 1280x1024 video in 16-bit SDR ITU-R BT.656 4:2:2 Mode 0.

    In free-run mode with blue background I get "0xFF00, 0x0000, 0xFF00, 0x0000..." pixel data, but it is 1280 LLC-period wide DE window between HSyncs…

  • LTC3300-2

    Hello everyone,

    I want to realize a communication between an LTC6804-2 and LTC3300-2 using the SPI that the first IC can generate.

    The problem is that the LTC3300-2 do not respond to the command I send to it, in particular I tried to send a 'Readback…