• RE: Load current of ltc3588 -2

    Hi Ashvajit,

    No, the max output current of the LTC3588-2 is 100mA.

    We don't have a piezo harvester that will output that much current, but you could possibly rectify the AC waveform to DC and use a solar charger.

    Regards,

    Zack

  • About LTC3588-1

    we bought the module of ltc3588-1 to solve the problem of triboelectric generator that is too small currnet to turn on led and charge the  capacitor. we connect our generator in pin PZ1 and PZ2. and next we connect our LED with pin VCC and GND. However…

  • 关于LTC3588

    这款芯片有一个功能,当电容上的电量积累到一定程度,后一级的DCDC就启动有输出,请问有没有相关电路图?

  • LTC3588-1 MODEL File

    I am conducting simulation work with the LTC3588-1 energy harvesting power supply.

    In order for my model to function, I need to use an ideal DC transformer, which is not available in LTSpice.

    Is there a .MOD file available that I can use to import the…

  • Wiring LTC3588-1 chips in series?

    Can two LTC3588-1 chips be mounted in series together so in theory an input voltage is split evenly across the two. More specifically can the PZ2 pin from chip one be connected to the PZ1 pin from chip 2 and then the unused pins be connected to the positive…

  • About the output function of LTC3588

    Hi,

    I have bought a LTC3588-1 demo PCB for triboelectric energy harvesting. Of course. it worked well.

    According to the experiment, I think it harvests energy from vibration and stores in a small capacitor, such as 10uF. Then LTC3588 transforms energy…

  • LTC3588-1, problem with the PGOOD

    I use the LTC3588-1 to charge a 33mF capacitor. The input Voltage is rectified and higher than 5 V and the charging current is higher than 500µA. The Energy Harvesting works but the PGOOD generates small peaks,  even before reaching the output voltage…

  • RE: About the output load of ltc3588

    My system is a sensor. I need a large current to ensure the transmission distance of the product. The system load is 150mA. Now ltc3588-1 works well on my system. It uses piezoelectric energy collection. I am thinking about whether I can store the output…

  • Could abandon PMOS and NMOS of LTC3588?

    Hi,

    I have bought a LTC3588-1 demo PCB for triboelectric energy harvesting. Of course. it worked well.

    According to the experiment, I think it harvests energy from vibration and stores in a small capacitor, such as 10uF. Then LTC3588 transforms energy…

  • 关于LTC3588样片的申请问题

    用学校邮箱在ADI官网注册成功后,申请LTC3588,显示未通过申请,请问如何能够通过申请,还是LTC3588这个芯片无法申请?