• LTC3586 Fault pin

    when LTC3586 Fault pin  is low ,  LTC3586 enable pin 1,2,3,4 was disable. 

    how can i do to ltc3586 enable pin work

    thank for your help

  • LTC3586 NTC obsolete

    Hi,

    I'm trying to implement the NTC function (0-45 degree cut-off) to my LTC3586 design, but I couldn't find the NTC on the datasheet online or for sale. The one I could find online that has similar P/N to the datasheet is "NTHS0603N01N1…

  • LTC3586 unused section

    If I'm not using one of the 4 regulators in the LTC3586, can I leave the associated pins open?

    Specifically, if pin 21, EN1 is tied to ground, can I leave pins 26 (SW1), 27 (VIN1) and 28 (FB1) floating?

    Also, am I correct there is no Spice model for…

  • LTC3586 電源問題

    您好

    當我的電池電源低的時候,LTC3586 FAULT PIN會導通到GND,讓LTC3586 ENABLE 1,2,3,4都失效。

    所以想請問當這種情況發生時,有沒有方法能讓FAULT PIN 關閉導通到GND。讓電源能正常工作?

  • RE: LTC3586-2 pin VBUS powered from battery

    Hello sir, 

    I am working on LTC3586 PMIC.i designed 4 layer pcb board. currently input supply is Type C usb with lLim (100mA) selection mode is '0'. in this condition the supply voltage is 5.1 V using USB and i received same (5.1V) at Vout pin. …

  • 智能可穿戴医疗保健设备解决方案

    先呈上完整资源包的下载链接:

    http://h.analog.com/CN-APM-WEARABLEff

    智能可穿戴医疗保健设备及典型架构

    可穿戴医疗保健设备可定义为能够自主监控或支持特定医疗功 能的无创式系统。(可穿戴的国家标准正在制定中) “可穿戴”一词说明该设备要么是直接佩戴在人体上的设备, 要么是一件衣服,并且具有适当的设计,支持其用作可穿戴配 件。广义上讲,这要求该设备具有极小的尺寸和重量,功能自 主,自备电源,易于使用,而且穿戴舒适。

    智能可穿戴医疗保健设备有多种类型,如腕带…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • LTC3586EUFEPBF

    用LTC3586EUFEPBF 做电源管理,LDO工作正常,其它4路不能工作,输出全为0。是什么@情况。