• LTC3550 Backup Time Calculation

    What is the reason that higher ESR causes less backup time when using the backup time calculator?

    Thanks.

  • LTM4644-1 LT POWER CAD 3+1 MODEL,

    CAN YOU POINT ME TO THE POWER CAD MODEL FOR 3+1, I ALREADY HAVE THE 2+2 AND 4.

    I WANT TO MAKE SURE I GET THE COMPENSATION VALUES CORRECT BEFORE BUILD.

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • RE: wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

    Hello,

    sometimes page one of the datasheet contains the answer:

    The LT8708-1 always operates as a slave to the master LT8708 and has the capability of delivering as much cur-rent or power as the master.

    Hence I would state, that LT8708-1 can NOT work…

  • AD4110-1 ADC issue

    Hi, I'm working on a project using AD4110-1.

    There are some things that I don't know using this chip.

    I know that

    1. SYNC Logic 'Low' means it will abort all ADC Operations

    2. SYNC Logic 'High' means it will start new conversion within…

  • For pin 1 orientation

    Hello respected,

    Have a good day....

    Please confirm pin 1 orientation on tape of package SOT223-3  and DFN-10 for below MPN.

    MPN = 

    LTC2854CDD#TRPBF = DFN-10
    LT1117CST#TRPBF = SOT223-3


    Thank you...

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • HMC666_using IF pin without 1:1 transformer

    Hello Team.

    1:1 transformer applied in IF pin is expensive.

    so we want to use without transformer.

    is it possible that?

    Can you support solutions?

    thanks.

    Best regards,

    Josh