• RE: .file_attr 1="1";

    Hi, Thanks for replying. I had tried the "-no-auto-attrs" with no improvement. The same error reappears elsewhere if I delete the source file causing the problem. It also occurs in the standard "BF609_init" project, so I have attached those files. The…

  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…

  • RE: LT3791-1 - EMI

    Hi Vagelis,

    EMI can be complicated with causes from component choices to board layout. It is very design dependent. I recommend that you contact ADI FAE in your area to help you out. 

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • ADF7030-1

    Hello,

    I bought the ADF70301 - 433 EZKIT and I can't find, in the ADF70301 data sheet, the noise figure of the transceiver. 

    So I'm here to ask: how can i measure the noise figure of the ADF70301 using the 433EZKIT?

    Thank you for your support

  • ad7656-1

    I'm requesting the gerber files for this product mentioned above... is it possible to receive them. thanks, 

  • LTC2439-1

    Hi!

    We wanna use the LTC2439-1 configured with 16-Channel Single-Ended Inputs, the Reference-Voltage is 5.0V and the Input-Channel Voltages are from 0-5.0V

    But the datasheet does not clearly describe the function for us with this configuration.

    We are not…

  • AD7988 - 1

    Good afternoon....

    I currently am using the above subject successfully in a design.  The power supplies are as follows: Vref = 2.5V, VDD = 2.5V and VIO = 2.7V - 3.6V.  Moving forward I would like to re-route the analog supply, VDD to track with VIO.  Can…

  • ADUM4121-1

    Can ADUM4121-1 gate drive handle 100% duty cycle?

  • LTC3300-1 problem with communication

    Hi everybody,

    I have problem with SPI communication between STM32 and LTC3300-1. I have only one LTC3300 and only one LTC6810. No IsoSPI, no DaisyChain. The ICs have separated CS/SS signals. I want to manage 6S Li-Ion battery pack. The literature, I have…