Is any more information available about using the LTC3407-2 in externally synchronized mode by feeding a clock signal to the MODE/SYNC pin? A general description of the synchronization mechanism would help answer several questions...
Specific questions…
Is there an Analog Devices part that can accept 4:4:4 encoding?
Hi
datasheet on page 13 states that the ADV7612 supports 36-bit 4:4:4 YCrCb, but the table 5 and 6 do not list this mode. Is it supported, how can it be activated?
best regards
Dani
I have a question. What is the content of Section AV for YCbCr 4:4:4 24 bit interface?
Page 13 of DS describes the PIXEL INPUT/OUTPUT FORMATTING The output section of the ADV7612 is highly flexible. The pixel output bus can support up to 36-bit 4:4:4 YCrCb or 36-bit 4:4:4 RGB. The pixel data supports both single and double data rates modes1…
Hello,
I wanted to ask for clarification on the VS and HS signals with the ADV7619 in pass through mode. i read the thread on this previously https://ez.analog.com/message/156902#156902 and it does say that the CP will be bypassed and the syncs remain…
We are using the ADV7627.
An error occurs when we have a source generating RGB 4:4:4. Output color is incorrect and exhibits lots of pink. When the source is connected directly to the display everything looks just fine. BTW, auto-CSC doesn't seem to…
Could you please provide the IIC configuration script for ADV7511 HDMI
I am working on the ADV7511 chip, which is the HDMI codec in VC707 EVB from
FPGA company Xilinx.
I want to configured the ADV7511 working in 1080P, 4:4:4 RGB input (each
component…
I started this question with my original post: ADV7627 RGB 4:4:4 Color Space Issue
Colorspace continues to plague my system and I am looking for some guidance. I have spent a considerable amount of time looking at the AVIAPI routines but there are some…
Hi we are looking for a video decoder which can convert PAL/NTSC composite, S-Video and YPrPb.Output format doesn't matter, it can be YCrCb 4:4:4 or RGB (it will go to FPGA so we can do any conversion).However all SDTV decoders I found only produce…