• s2p  file for HMC921LP4E reference at 1-1.2 GHz.


    Hi,

    I am working on a new design and need s2p file for HMC921LP4E Power amplifier. I am looking at 1-1.2 GHz  frequency range, need s2p parameter for simulation purpose. I would appreciate if someone can help, need it quite urgently. Thanks in advance…

  • latest source code release of the ALICE 1.2 desktop

    Hello again,

    The wiki-page with the ALICE User’s Guide https://wiki.analog.com/university/tools/m1k/alice/desk-top-users-guide points for the latest source code release of the ALICE 1.2 desktop tool to  https://github.com/analogdevicesinc/alice/releases…

  • RE: ADISIMPLL problem

    The VCO in the ADF4360-7 can only cover a frequency range with Fmax/Fmin < 1.2. The exact centre frequency is set using Lext.  So whilst the ADF4360-7 can be used over the entire frequency range, any individual design cannot cover a frequency range…

  • RE: A problem with AD-FMCDAQ2-EBZ FMC Board

    The revision numbers of AD-FMCDAQ2 is shown as the picture,

    I'm not good at Linux, so I don't know whether what post here is your need.If it is not ,please tell me .Thanks!

    root@xkw-HP-ProBook-4421s:/home/xkw# dmesg | more

    [ 1835.804929]…

  • RE: AD-FMCOMMS1-EBZ REV B testing problems based on Xilinx_kc705

    Hi,

    I've just done a test using a KC705 revision 1.2 (the changes from rev. 1.1 to 1.2 are minor: AR# 59751 - Kintex-7 FPGA KC705 Evaluation Kit - Changes from rev 1.1 to rev 1.2) and everything works fine.

    Your board gets stuck during the DMA configuration…

  • RE: ADA4941

    前级增益 = 1 + (1/4.99) = 1.2

    后级增益 = -1

    总增益1.2

    1.701 / 1.414 = 1.2

    显示结果正确,没有问题

    你这2.4的增益如何获得的?

  • USBi 1.3 problem

    My USBi 1.2 is working properly on Windows 7 / 64 , USB 2.0 port

    The USBi 1.3 ( delivered with ADAU1452 ) is not recognized properly , driver won't install.

    Any help ?

    Will the ADAU1452 wotk with USBi 1.2 ?

    At the moment download bar shows green…

  • RE: ADA4932 Vocm and SPICE model issue

    Hi buckd,

    ADA4932's Vocm is specified to be −VS + 1.2 to +VS − 1.2 when operating at Vsy=5V. This will translate to 1.2V to 3.8 V operating range. With that being said, Vcm=0.9V will definitely won't work.

    Regards,

    Jino

  • RE: after following the no-os setup I was able to get the build done without errors but when I run I get the error "RX MMCM-PLL NOT locked TX MMCM-PLL NOT locked  RX OS MMCM-PLL NOT locked  clkgen_setup() failed"

    In this case, try first to rebuild the Vivado project using your revision number instead of 1.2. If it doesn't solve the issue, we have to find out all the differences between revisions 1.2 and 2.0.

    Let us know how it goes.

    Thanks,

    Dragos

  • RE: ADP1048 for 2kw solution

    So far , Does ADP1047/48 could meet the PMBUS 1.2 function ????

    READ_EIN And READ_EOUT

    • Revision 1.2 Will Have Two New Commands:

    READ_EIN And READ_EOUT

    • Attempt Is To Make Reporting Of Power

    – Independent Of PMBus Device Characteristics

    – Put…