• ADP5071 2 A/1.2 A How to achieve

    hi,I use Input power 5V4A,want to get ±6V,1.5A,but I use ADP507x_DesignerTools,Remind me the maximum current is 1.25and.37,What am i doing wrong?

  • ADM7170 - Vout 1.2 V

    Hi,

    I'm planning to use the ADM7170 as 1.2 V voltage source. According to the datasheet ordering guide table (page 23/23), the adjustable models (ADM7170ACPZ-R7 & ADM7170ACPZ-R2) are listed with an output voltage of 1.2 V.

    As stated on page 16…

  • date code for LTC3406BES5-1.2#TRMPBF

    please decode the date code for the following part

    LTC3406BES5-1.2#TRMPBF

  • RE: LT6106 MTBF/MTTF data

    The reliability report on the website indicates the FIT for these to be better than 1.2, or MTBF of 95,000 years.

  • RE: Gain/Reading error

    Here my code :

    fADC0RESULT = ADC0DAT * 1.2/268435455;

    uiDACdata = fADC0RESULT / (1.2 / 4095.0);

    DACDAT = uiDACdata << 16;

  • Chip Revision identification

    I receved TigerSharc chip:

    ADSP-TS201S
    ABP-050
    706543.1-D-1.2
    0528 CANADA

    Could you tell me what silicon revision this is?

     

    The device you have is silicon revision 1.2, which can be read from the string:
    706543.1-D-**1…
  • AD6688 Data Capture in 1.2 GHz BW Mode

    I am capturing data using the AD6688 Eval Board and ACE software with the following  settings :

    NCO frequency set to 1 GHz 

     I apply 4.1 GHz , 10 dBm tone signal. Against my expectation the  the signal has a component at the image frequency (- 100 MHz).  Following…

  • Sleep command in UBOOT 1.2 for SC589 EZ KIT.

    Just want to confirm the following behavior:

    If I type sleep 20 in U-boot, it actually 40 seconds..

    ACS

  • RE: ADP151AUJZ-1.2-R7 Part code information.

    Hi P.konstantinov,

    #- means the part is lead free and QN refers to the date code which means that the part produced sometime on April to May 2017.

    Cheers,

    Alex

  • s2p  file for HMC921LP4E reference at 1-1.2 GHz.


    Hi,

    I am working on a new design and need s2p file for HMC921LP4E Power amplifier. I am looking at 1-1.2 GHz  frequency range, need s2p parameter for simulation purpose. I would appreciate if someone can help, need it quite urgently. Thanks in advance…