Here is a file I was unable to post earlier.
DOCX
Hi,
I'm planning to use the ADM7170 as 1.2 V voltage source. According to the datasheet ordering guide table (page 23/23), the adjustable models (ADM7170ACPZ-R7 & ADM7170ACPZ-R2) are listed with an output voltage of 1.2 V.
As stated on page 16…
please decode the date code for the following part
LTC3406BES5-1.2#TRMPBF
Can't to read part code ADP151AUJZ-1.2-R7.
#ON what does it mean?
Q: Can HMC936A operate below the specified frequency range?
I installed the executable ALICE 1.2 software on a Windows 10 64 bit machine. All of the tools work fine EXCEPT the dc meter-source 1.3 tool. When I open it and click the RUN dot box, the app window fades a little and then the (not responding) message…
Low power HDMI 1.2 Compliant AD9889B Tx configured as slave (default) not detected by the I2c bus interfaced to McASP0 .
hi,I use Input power 5V4A,want to get ±6V,1.5A,but I use ADP507x_DesignerTools,Remind me the maximum current is 1.25and.37,What am i doing wrong?
I am capturing data using the AD6688 Eval Board and ACE software with the following settings :
NCO frequency set to 1 GHz
I apply 4.1 GHz , 10 dBm tone signal. Against my expectation the the signal has a component at the image frequency (- 100 MHz). Following…
Hello again,
The wiki-page with the ALICE User’s Guide https://wiki.analog.com/university/tools/m1k/alice/desk-top-users-guide points for the latest source code release of the ALICE 1.2 desktop tool to https://github.com/analogdevicesinc/alice/releases…