• 2*2 MIMO setup

    Hello,

    Iam interested in implementing a MIMO 2*2 scenario where i will use 2 fpgas (1 as the transmitter and 1 as the receiver) where each one  will be connected with one AD-FMCOMMS3-EBZ.
    So the setup will be :
    FPGA_1 + AD-FMCOMMS3-EBZ_1 =Base stati…

  • RE: 2 shunts to measure 2 loads with ADE7953

    Hi ,

    Yes you can do that.

    The current channel A and B can be populated with Shunt Resistors for each load. Usually the channel B is used to monitor the neutral current in billing or to detect tampering. I assume there is no tamper detection needed…

  • 4:2:2 8bit ycrcb

    Hi,

    I have the EVAL-ADV7612-7511p video evaluation board .I'm using 7612 to receive  HDMI inputs from camera(720p @60) , and then feed to 7511 to output the video to the screen. 

    camera -> 7612 --> 7511 --> screen

    When adv7612 output 4:4:4 8bit ycrcb…

  • ADV7610 registers 4:2:2

    Hello

    Thanks in advance.

    I have a input video signal whose format is: YCbCr (Digital YUV) 20 bit (10 chroma + 10 luma).. 1080p60 (1920x1080 60 fps).

    As I can read in this forum ADV7610 only supports four modes for SDR 4:2:2:

                     - 8 bit SDR ITU-R BT.656…

  • ADV7403 YUV 4:2:2?

    Can the ADV7403 output YUV 4:2:2 rather than YCbCr 4:2:2?

    Thanks.

    Chris

  • Connect with 2 jtags to 2 Processors

    I'm trying to connect with 2 jtags to 2 processors , BF547 and BF512, at the same time with no succes.

    I have no Problem to connect to each one of them separatly.

    I know that it's Posible to connect to 2 processors at the same time .

    Do you…

  • Question about ADM1172-2

    Dear ADI Expert,

    My customer uses ADM1172-2 for output short circuit test. The waveform of Output / Gate / Timer is not the same as the datasheet. The datasheet waveform is shown in Figure 1. My customer test results are shown in Figure 2. After the output…

  • RE: LTC6804-2 and LTC6811-2 reference voltage 1 and 2 at 0V.

    I'm having this same exact issue with the LTC6813 as well. The SPI communications work and a valid PEC is received always, however, the values themselves are 6.5535V and the REF voltages are always at 0V. 

    https://ez.analog.com/power/f/q-a/104495/ltc6813…

  • RE: JPEG Processing - 4:2:2 v 4:2:0?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,