• latest source code release of the ALICE 1.2 desktop

    Hello again,

    The wiki-page with the ALICE User’s Guide https://wiki.analog.com/university/tools/m1k/alice/desk-top-users-guide points for the latest source code release of the ALICE 1.2 desktop tool to  https://github.com/analogdevicesinc/alice/releases…

  • s2p  file for HMC921LP4E reference at 1-1.2 GHz.


    Hi,

    I am working on a new design and need s2p file for HMC921LP4E Power amplifier. I am looking at 1-1.2 GHz  frequency range, need s2p parameter for simulation purpose. I would appreciate if someone can help, need it quite urgently. Thanks in advance…

  • Sleep command in UBOOT 1.2 for SC589 EZ KIT.

    Just want to confirm the following behavior:

    If I type sleep 20 in U-boot, it actually 40 seconds..

    ACS

  • Differences between SC589 EZ rev 1.1/BOM1.6 and Rev 1.2/BOM1.8

    I recently upgrade to Sigma Studio for Sharc 3.9.0 and have hit a hardware compatibility issue. Details on that can be found here: SS for Sharc 3.9.0 and SC589 EzBoard version issues 

    In looking at the ADI website for the SC589 board:

    www.analog.com…

  • power-up sequencing for giving 3.3V and 1.2 V input supplies to ADSP-BF536/7

    I am using a dual supply LDO regulator with power-up sequencing
    for giving 3.3V and 1.2 V input supplies to ADSP-BF536/7. This regulator has a
    power up sequence and gives 3.3V o/p first and 1.2V follows. Do you see any
    problem with this…
  • how can i generate pure sine wave of 1.2 khz and 2.2khz using aduc7026 controller by 12 bit dac...

    i am having one code where it is using look up table of various samples generating 10khz frequency but i am not getting how to generate for 1.2khz and 2.2.khz

  • How can we restrict the bandwidth of ADXL203 to 0.6 to 1.2 Hz only and how can we set the analog o/p scaling to 0 to 1m/sec2?

    How can we restrict the bandwidth of ADXL203 to 0.6 to 1.2 Hz only and how can we set the analog o/p scaling to 0 to 1m/sec2?

  • 有没有5伏/3.3伏无负载时静态工作电流小于1.2毫安的带隔离器件和相应的应用电路设计

    各位大虾:

    有没有5伏/3.3伏无负载时静态工作电流小于1.2毫安的带隔离器件和相应的应用电路设计

  • RE: ADA4941

    前级增益 = 1 + (1/4.99) = 1.2

    后级增益 = -1

    总增益1.2

    1.701 / 1.414 = 1.2

    显示结果正确,没有问题

    你这2.4的增益如何获得的?