• TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • RE: ADV7619:SDR 4:2:2 Output Modes 16Bit,can support resolution 4K@30Hz,another word,can clk up to 297MHz

    Thank you for your reply!

    TXT is  ADV7619 register configurition,under that configuration,MCU can not get any data from the output

    The pdf is  ADV7619 hardware schematic diagram。

    Under these condition,can make 4k@30Hz work without change ADV7619 hardware…

  • LT3470A

     PDFHi,

    I am Facing one problem with module LT3470A.

    This module configured as buck converter which will give 2V constant output at input range of 6V to 20V.(load less than 50mA)

    As per the data sheet pins are configured. This is my typical design.(Here…