• RE: HMC858 Vil Vih

    Hi,

    Please find the attached application note explaining interfacing of  high datarate and high speed logic parts.

     PDF

    Best regards

    Sinan

  • Use ADM1062's ADC from inputs VX1-5, VP1-4, VH & Temp sensor without averaging?

    Can I use the ADM1062's ADC from inputs VX1-5, VP1-4, VH and Temp sensor
    without averaging?
    I don't want to use the EEPROM for configuration. I want to initialize the
    ADM1062 every start up over the SMBus. Can you tell me which…
  • RE: LVDS25/LVPECL driving a HMC723LP3

    Hello ffrank,

    LVDS25 has a common mode voltage of 1.25V with swing between 1.075V and 1.425V. If you shift voltages of HMC723 from GND/-3.3V to 1.425V/-1.875V, that would solve your issue. Please refer to the page 18 of the application note I attach…

  • 11/16/16 The Art of Military Communications

    This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…

  • 2020年 ADI 20款硬核新品,为你献上电路设计的不二之选

    你最关注的领域是什么?ADC/DAC?Power?RF?.....

    你知道ADI在这些领域都推出了怎样的硬核新品吗?

    回首2020年,虽然被疫情干扰,不过咱ADI依旧没有停止推出新产品的脚步,今天斑竹就为大家盘点一下今年的“新秀”吧~

    四通道、软件可配置输入/输出 AD74412R/13R

    AD74412R 是一款适用于楼宇和过程控制应用的四通道软件可配置输入/输出解决方案。AD74412R 包含用于模拟输出、模拟输入、数字输入和电阻温度检测器 (RTD) 测量的功能,这些功能集成在一个单芯片解决方案中…

  • 3-4月ADI新品主打,快来康康有没有适合你的设计~

    携一缕浅夏的芬芳,凝一脂冰清玉洁的清梦

    各位小伙伴们,迷人的仲夏五月来啦~

    在这个似水的季节里,悠然翻阅学习岂不美哉?

    今天斑竹给大家带来 ADI 3 - 4月的新品合集,想要了解学习的筒子可千万不能错过哦~

    MxFETM四通道 16 位 12GSPS RFDAC 和双通道 12 位 6GSPS RFADC AD9082

    发射信号前端 (MxFE®) 是一款高度集成的器件,具有 16 位、12 GSPS 最大采样率射频 (RF) 数模转换器 (DAC) 内核和 12 位、6 GSPS 采样率…

  • RE: TCXO 122.88 MHz reference

    Hi ,

    The TCXO product id can be found in the BOM section in the EV-ADF4355-3SD1Z user guide...I have attached the datasheet for it, regards,

    Brigid.

  • 在新年到来之际,送你一组钻石级硬度的精选硬核产品吧~

    转眼间,2020年就要结束了,今年你都做了些什么呢?

    对于ADI,我们可是推出了不少硬核产品哦~

    今天,斑竹就给大家晒晒ADI这些杠杠滴成果!

    -------------------------------------------------------------------------

    软件可配置的四通道输入/输出 AD74413R

    AD74413R是一款软件可配置的四通道输入/输出解决方案,适用于楼宇和过程控制应用。AD74413R包含用于模拟输出、模拟输入、数字输入、电阻温度检测器(RTD…

  • LT3470A

     PDFHi,

    I am Facing one problem with module LT3470A.

    This module configured as buck converter which will give 2V constant output at input range of 6V to 20V.(load less than 50mA)

    As per the data sheet pins are configured. This is my typical design.(Here…

  • 实力支招,这七个应用的传感器可以这样选

    加速度计能够测量加速度、倾斜、振动或冲击,因此适用于从可穿戴健身装置到工业平台稳定系统的广泛应用。市场上有成百上千的加速度计器件可供选择,其成本和性能各不相同。最新MEMS电容式加速度计应用于传统上由压电加速度计和其他传感器主导的应用领域。新一代MEMS加速度计可为CBM、结构健康监控(SHM)、资产健康监控(AHM)、生命体征监测(VSM)和物联网无线传感器网络等应用提供解决方案。然而,在有如此多加速度计和如此多应用的情况下,选择合适的加速度计并非易事。

    尚无行业标准界定加速度计属于何种类别。加速度计的一般分类及相应的应用如表1所示…