您好 我应用咱家LTC3355电路芯片 并将其搭配电路使用后,发现当我的输入为6V的情况下,其输出侧只有0.34V,测量电压发现Vin端子仅有2V左右,
相关元器件细节为,D1选用的 是IN4007,D2选用的 是SR260,LI为4.7μH,您看下是我这边电路是设计有问题吗,麻烦啦?
您好 我应用咱家LTC3355电路芯片 并将其搭配电路使用后,发现当我的输入为6V的情况下,其输出侧只有0.34V,测量电压发现Vin端子仅有2V左右,
相关元器件细节为,D1选用的 是IN4007,D2选用的 是SR260,LI为4.7μH,您看下是我这边电路是设计有问题吗,麻烦啦?
Hi,
As per the datasheet of LTC3355, the charge current of the Super capacitor is in the range form 0.1A to 1A.
Kindly provide the necessary information about the operating condition & stage of the Vout and Supercap, If the power available at the input…
It's better to measure the I/V curve at your nominal operation condition which means under the nominal primary current.
If the I/V curve is your nominal operation condition, you will waste a lot of energy by limit the voltage lower than 3.3V. But…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |