电路图如附件所示, 6脚vout输出电压低于11脚vin的电压0.5V左右 为什么?
Hello,
small output currents:
https://www.analog.com/en/products/ltc3260.html#product-overview
Larger currents than 100mA:
https://www.analog.com/en/products/lt8471.html
kind regards
Markus
Hello,
Do you need all three solutions or just the 12V input to -12V output 1.5A?
I would suggest using a micromodule. LTM4651 is an option for this.
Edit: For the (-12V) to ±5V (adjusted output). 0.1A max
ganging up 2 LTC3260 should be able to…
an LMThat's it. When I use the LTC3260 appear the problems but not with a supply using two linear regulators (LM 317 / 337). When supply is linear all works fine.I will ask for a power supply solution.
Thanks a lot.
Hi
I am FAE in Japanese distributor.
Our customer looks for power controller of HMC-AUH312.
Is LTC3265 or LTC3260 possible to drive VDD and VGG1?
If VDD and VGG1 needs Bias controller, could you please tell me the part number?
Best regards
N.Kokubo
Thank you, I will definitely attention this issue.
What About the PM? Is the LTC3260 adequate? do you have any better proposals ?
regards,
G.
Bad CRC samples occured like every 20 s. In the tests and figures above the bad samples were discarded. So yes, the dataset is reliable.
The SPI interface is now stabalized by extra strong drive strength of the SDO. Yet this did not change the high-noise…
一)LTC326x/LT858x/ADP507x/ADP505x,这几个型号重点了解一下呢。
https://www.analog.com/cn/products/ltc3260.html
https://www.analog.com/cn/products/lt8582.html
https://www.analog.com/cn/products/adp5052
https://www.analog.com/cn/products/adp5070
二)7.4V锂电池,也需要开关DC/DC充电的吧…
Hi, Karen, I've already used the documents you suggested. My (actual) problem is only the power supply.
I know the schematics for the evaluation board, but they are not specific enough for me, to see how they solved the power supply problem.
I…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |