• JPEG Processing - 4:2:2 v 4:2:0?

    My JPEG saga continue...

    I am using a BF561 single core to compress a 640x480 YUV 4:2:2 image into JPEG format, employing the ADI JPEG Library tools.  I am getting very poor performance compared with the reference results from the Spec Sheet.  The Spec…

  • ADV7842 4:2:2 DDR mode, ADV7393: Stanag3350 support?  (2)

    Hello Dave,

    I am facing problems with replies to your answer, so I am oppening a new dicussion with the same title.

    Please clarify your answer regarding STANAG support:

    2) As I understand it, this is the same as RS-343A/EIA-343A and none of our parts…

  • LTC6804-2 and LTC6811-2 reference voltage 1 and 2 at 0V.

    Hello,

    I installed 2x LTC6811-2 and then 1x LTC6804-2 on the same board and I don't have any voltage reference output at anytime. The functional diagram in the datasheets shows that VREF1 should be always present as it's generated from V+. VREF2 is not…

  • 2*2 MIMO setup

    Hello,

    Iam interested in implementing a MIMO 2*2 scenario where i will use 2 fpgas (1 as the transmitter and 1 as the receiver) where each one  will be connected with one AD-FMCOMMS3-EBZ.
    So the setup will be :
    FPGA_1 + AD-FMCOMMS3-EBZ_1 =Base stati…

  • RE: ADA4807-2

    你输入信号的幅度为多大?我猜测你输入的信号过大,再乘以过高的增益后,输出达到电源轨,以致饱和。

    所以你需要先查一查你的输入信号的幅度。

  • ADV7403 YUV 4:2:2?

    Can the ADV7403 output YUV 4:2:2 rather than YCbCr 4:2:2?

    Thanks.

    Chris

  • 4:2:2 8bit ycrcb

    Hi,

    I have the EVAL-ADV7612-7511p video evaluation board .I'm using 7612 to receive  HDMI inputs from camera(720p @60) , and then feed to 7511 to output the video to the screen. 

    camera -> 7612 --> 7511 --> screen

    When adv7612 output 4:4:4 8bit ycrcb…

  • ADV7610 registers 4:2:2

    Hello

    Thanks in advance.

    I have a input video signal whose format is: YCbCr (Digital YUV) 20 bit (10 chroma + 10 luma).. 1080p60 (1920x1080 60 fps).

    As I can read in this forum ADV7610 only supports four modes for SDR 4:2:2:

                     - 8 bit SDR ITU-R BT.656…

  • RE: ADIS16497-2 command

    Hi ,

    Sorry for the late reply. 
    It is the second. Write low byte, stall 340 us then write high byte.
    But please do note that the ADIS16497 can take up to 20 ms to execute a write command to the FNCTIO_CTRL Register. 

    Hope this helps. 

    Best regards,
    J…

  • YCbCr 4:2:2/12 ADV7619

    When I input YCbCr 4:2:2/12 into my ADV7619 and readi back 0x0B(DEEP_COLOR_MODE) of the HDMI map it always reports 8 bits per channel.  I also see this on the eval board as well.  While YCbCr 4:2:2/10 is reported correctly.

    Is there some conversion in…