Hi!We use LTC3118 in our system for the voltage buck converter/battery back-up because of its dual power path facility. The output voltage is 5V. The input voltages are 12V and 3.6...4.1V (Li-Po battery).
We used the same design in previous PCB production…
Hi,
I am using the ltc3118 in a battery-powered device. Because of that, I want to use it in burst mode. I used the typical application note from the datasheet. IN1: 18V wall socket, IN2: Battery pack 12V, OUT: 5V. With almost no load the voltage is quite…
Hi
I have tested the LTC3118 by a single power supply from 3.6V to 7.2V, the output voltage is 5V. I have used the Vin1 pin as the voltage source for the converter. My question is that where the unused Vin2 pin and the Run2 pin are connected to. I have…
Hi Bell,
The closest item I can find is the LTC3118. Please check specs in our website.
Current sharing is difficult in LTC3126 as it doesn't have an external Vc pin like LTC3118. We can control the inductor current level with this pin.
Paralleling LTC3126 with additional current sensing and load sharing circuitry might not be a…