• LTC3115-2 Protections

    Hello!

    We have a LTC3115-2 that has a nominal 28V input and a nominal 28V output. It should be noted that we are trying to power the converter into a 750uF output capacitance (the 9ms soft start time is nowhere near enough). For a while, we saw no issue…

  • LTC3115-2仿真

    您好,我使用LTspice XVII对LTC3115-2进行电路仿真,采用数据手册中推荐的参考电路方案,但仿出来的波形很奇怪,不知道问题出在哪里,请给予帮助和解答。谢谢!

  • use LTC3115 for variable power supply

    Hi,

    I want to make a variable power supply controlled by a microcontroller (stm32f767zi).

    The input voltage will be 24V. The output voltage should be adjustable (via the microcontroller) between 14V and 31V.

    The output current is maximum 0.8A.

    Can…

  • LTSpice small signal model as referenced in the LTC3115-2 datasheet

    Hi,

    The applications information section of the LTC3115-2 datasheet references use of a Bode plot generated in LTspice from the small signal parameters of the LTC3115-2.  Is the LTspice model available for customer use when calculating compensation loop…

  • LTC3115电源芯片静态功耗问题

    官方手册上ltc3115静态电流只有30uA,实际我按照官方给的原理图电路,输出12V电源,不接负载时候,输入12V输出12V静态电流达到26mA,,与官方给的参数相差1000倍

  • LTC3115的EVM板输出为5V,这个5V可以直接给手机供电吗?(DC2119为EVM板)

    LTC3115的EVM板输出为5V,这个5V可以直接给手机充电吗(输入变化范围为3-12V)?(DC2119为EVM板)

  • LTC6363-1 replacement LTC6363-1 replacement LTC6363-1 replacement

    Hi,

    Is there any alternatives to LTC6363-1 since it is out of stock? 

    I need a single to differential Amplifier with a fixed gain of one. It is used in a current sensing circuit.

    Regards,

    Mamzi

  • ADA4857-1 1 to 4 fanout

    Dear Sir/Madam,

    I am after some PCB routing advice on connecting one ADA4857-1(gain of 2) to four ADA4857-1 (gain of 1).
    The delay between the ADA4857-1 is not important just signal quality.

    Regards Joe

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…