• LTC3109 input component parameters

    Hello
    What are the parameters of LTC3109 C1A(C1B), C2A(C2B), T1 (T2) at the input voltage AC Vrms=0,08-1,3V Iin=0,4-42mA Isource=19Ohm?
    Thanks.

  • LTC3109 shunt harvesting

    Dear all,

    I made a pcb design to harvest energy from a voltage drop (>20 mV) that occurs in a trace i have in my PCB. This trace carries 2 A and runs on the bottom layer.

    However, it does not work. Has enyone tried this already? Could it be that…

  • RE: PCB design for LTC3109 - TEG energy harvesting

    I Think there should be at least 2uF capacitor on VLDO pin. Did you find the problem?

  • RE: LTC3108 for small scale electromagnetic generator

    Another question I have. What is the significance of a transformer at the input pins of the LTC3109. Would that be necessary or can I just connect my low voltage AC generator directly to it without any transformers?

    Many thanks

  • Simulating LTC3108 in LTspice

    My name is João Cláudio and I'm a student of Electrical Engineering. I'm trying to simulate the LTC3108 with a programmed Vout of 5V. But, if I do that, Cstore never starts to charge. When Vout reaches 4,98V it gets stuck in this voltage and…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • 【在线研讨会】ADI技术及产品支持中国能源互联网

    4G改变生活,5G改变社会。5G技术正加速推动互联网进入下半场,即产业互联网,而能源互联网将是产业互联网的最重要应用领域之一。能源互联网可理解是综合运用先进的电力电子技术, 信息技术和智能管理技术, 将大量由分布式能量采集装置, 分布式能量储存装置和各种类型负载构成的新型电力网络、石油网络、天然气网络等能源节点互联起来, 以实现能量双向流动的能量对等交换与共享网络。

    在能源互联网时代,任何一个微小的安全漏洞,都可能导致大批风电场和光伏电站陷入瘫痪,或是自动驾驶的电动汽车改变路线。推进能源数据安全监测与防护保障能力建设已迫在眉睫…