• LTC3108-1

    Hi,

    We are working on PoC based on LTC3108-1. We wish add a LED for visual monitoring, LTC3108 is not able to supply a suffisient current to drive the LED.

    Could we use C2 input for drive an external Mosfet (low Qg) ?

    BR

    Benjamin

  • Energy Harvesting using LTC3108

    Hello,

    Im planning to make an energy harvester using LTC3108 in which we use a Patch Rectenna. Our goal is to charge a mobile phone obtained from the surrounding radio frequencies. The antenna will operate in the range of 0.85Ghz to 10.6Ghz. Wanted to…

  • LTC3108

    Can anyone please give me some help that what is the output current of LTC3108?? & is it continious  in nature or only occurs for a very short period of time?? plzzzzzzzzzzzzzzzzzzzzz help me or give me suggest me some alternative for this to convert…

  • RE: LTC3108 for small scale electromagnetic generator

    Hi,

    The transformer is needed to boost the input voltage and together with the capacitor its forms a self resonating converter.  You can use the part without transformer if the input voltage is high and in that case there will be no boosting. (Page 20…

  • Simulating LTC3108 in LTspice

    My name is João Cláudio and I'm a student of Electrical Engineering. I'm trying to simulate the LTC3108 with a programmed Vout of 5V. But, if I do that, Cstore never starts to charge. When Vout reaches 4,98V it gets stuck in this voltage and…

  • LTC3105 & LTC3108 for thermoelectric generator

    Hello.

    I want to boot output voltage of thermoelectric generator (TEG).

    I had successfully used LTC3108 for voltage booster using low impedance peliter TEG.

    But the LTC3108 didn't work well, when I connected high impedance TEG.

    I saw some article…

  • LTC3108 vs BQ25570 (from TI)

    Hello,

    I have made a board using a BQ25570 (from texas instrument) able to harvest solar energy from a solar panel (0.42W-3V) and to recharge two 35F suparcap and then providing 3.3V to my main board that can send radio frames over sigfox network. This…

  • Ultra low power source for LTC3108

    Hello,

    I am evaluating the LTC3108 with a prototype TEG that provides 20-50mV but has a very low power rating (around 1uW).

    Initial experiments indicated that at least 300uW of power are required by the LTC3108 in order to start-up and provide voltage…

  • LTC3108的TEG曲线

    Hi

         I want to measure the "IOUT vs dT and TEG Size" curve, but I don't know what equipment to use to ensure a stable temperature difference. Can you give me some suggestions?

    Thanks!

  • LTC3108仿真与提升效率

    我需要对整个系统(包含其他芯片)的运行进行仿真,但是官网没有提供LTC3108pspice模型(只有LTspice);

    请问有没有LTC3108pspice模型,或者是能协助我搭出pspice模型的原理分析,参考文献或参考文档;主要是不知道3108入口处的管子(如下图所示)是怎样开始驱动的,那是个什么样的管子。

    现在的效率还达不到我们的要求。在不更换芯片的前提下,是否有方法提高效率。

    从芯片本身来讲,什么限制了芯片效率?