• RE: Simulating LTC3108 in LTspice

    Please do SYNC RELEASE in LTspice. The model has been updated. Thanks!

    Best Regards,

    Hong

  • RE: Energy Harvesting using LTC3108

    one can use only with AWR  tool alone

  • Ultra Low Switched Capacitor Pump like LTC3108 LTC1502-3.3

    Hello,

    Is it possible for one of your voltage step-up products to cold start/operate from ultra low Vin, like your LTC3108, but instead of using transformers/inductors, that the product be entirely switched capacitor based? Your LTC1502-3.3 is switched capacitor…

  • LTC3108-1

    Hi,

    We are working on PoC based on LTC3108-1. We wish add a LED for visual monitoring, LTC3108 is not able to supply a suffisient current to drive the LED.

    Could we use C2 input for drive an external Mosfet (low Qg) ?

    BR

    Benjamin

  • LTC3108的TEG曲线

    Hi

         I want to measure the "IOUT vs dT and TEG Size" curve, but I don't know what equipment to use to ensure a stable temperature difference. Can you give me some suggestions?

    Thanks!

  • LTC3108

    Can anyone please give me some help that what is the output current of LTC3108?? & is it continious  in nature or only occurs for a very short period of time?? plzzzzzzzzzzzzzzzzzzzzz help me or give me suggest me some alternative for this to convert…

  • LTC3108 for small scale electromagnetic generator

    Hello, I'm building a small scale vibration energy harvester made up of coils and magnets (electromagnetic generator). The generator currently produces an output in the range of 0-300mV AC. I was wondering whether the LTC3108 will be suitable for this…

  • LTC3105 & LTC3108 for thermoelectric generator

    Hello.

    I want to boot output voltage of thermoelectric generator (TEG).

    I had successfully used LTC3108 for voltage booster using low impedance peliter TEG.

    But the LTC3108 didn't work well, when I connected high impedance TEG.

    I saw some article…

  • LTC3108仿真与提升效率

    我需要对整个系统(包含其他芯片)的运行进行仿真,但是官网没有提供LTC3108pspice模型(只有LTspice);

    请问有没有LTC3108pspice模型,或者是能协助我搭出pspice模型的原理分析,参考文献或参考文档;主要是不知道3108入口处的管子(如下图所示)是怎样开始驱动的,那是个什么样的管子。

    现在的效率还达不到我们的要求。在不更换芯片的前提下,是否有方法提高效率。

    从芯片本身来讲,什么限制了芯片效率?

  • Ultra low power source for LTC3108

    Hello,

    I am evaluating the LTC3108 with a prototype TEG that provides 20-50mV but has a very low power rating (around 1uW).

    Initial experiments indicated that at least 300uW of power are required by the LTC3108 in order to start-up and provide voltage…