• LTC3026 - Best Way to Sequence ON and OFF

    I get this question a lot, so I will ask the question in a post and answer myself.

  • LTC3026 BST for how many others LTC3026 ?

    Hello,

    According to the datasheet "the boosted output voltage of one LTC3026 can supply the boost voltage for other LTC3026s" 

    But how many maximum can we connect ? Is there any limits/requirements to do so ?

    (My application required 5x LTC3…

  • LTC3026的SW管脚悬空还是接地?

    LTC3026这款芯片的SW管脚在最新的手册里面通过悬空来disable boost converter,但是之前版本的手册都是通过接地来实现的,如果使用旧的接法会对芯片造成什么影响吗?

  • 热门必看丨ADI Power的20个问答帖,你想知道的都在这儿

    各位筒子们,又到了这个月的热门问答帖时间~

    这次,为大家带来的是来自咱们中文论坛的ADI Power系列问答20则!这些问答都由ADI工程师精心解答,绝对干货满满~

    好啦,话不多说,咱们开始吧

    问题一、LTC4162-L42充电功能异常应该如何解决?

    ez.analog.com/.../ltc4162-l42

    问题二、LTC3891IFE调整电阻使输出电压为5V,输出电流可以达到多少?

    ez.analog.com/.../ltc3891ife-5v

    问题三、LTC3026的SW管脚应该悬空还是接地…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • RE: ADV7619 EDID registers

    Hi Poornima,

    My question is more simple. I didn´t try to do it yet because I don´t know how I could do it, that is my question. I saw in the schematic (which I attach you) that the RX0_DDC_SCL and RX0_DDC_SDA belong to the HDMI cables but also are connected…

  • LT 3033 malfunctioning

    Hello,

    I am trying to test the IC : LT 3033. It has a linear regulator with a internal reference voltage of 0.2V. I had set feedback resistors of 150K and 11k to expect an output of 2.9V approx. However I am getting an output voltage of 0.48V at a supply…