I used the circuit shown here to get 3.3V.However, the actual output is 3.0V.So I want to know where did I go wrong.
I used the circuit shown here to get 3.3V.However, the actual output is 3.0V.So I want to know where did I go wrong.
If the LDO get an enable input before the VIn and Vbais - is it cause any problem or any unwanted operation?
I need the ability to regulate two voltages (2.7V & 3.1V) for a single power supply. I was planning on using the LTC3025-1 and wanted to know if it was possible to connect two of these regulators outputs together but only enable one regulator to get…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |
Hello,
I am trying to test the IC : LT 3033. It has a linear regulator with a internal reference voltage of 0.2V. I had set feedback resistors of 150K and 11k to expect an output of 2.9V approx. However I am getting an output voltage of 0.48V at a supply…
作为电子电路的基本构成,电源可以说无处不在,通信、汽车、消费类电子……
当今时代,电源广泛应用于各种热门的市场应用之中,并成为其必不可缺的一个重要组成部分。
作为工程师,在电路设计中不可避免的会遇到电源技术的难题
今天,斑竹为各位小伙伴带来了ADI工程师亲自盘点的ADI Power的技术问题集,希望能够帮到大家哦~