Hi Logan,
About the way to speed up by using two LTC2986s, how can I get 12ch in 1s since this part's ODR is 164ms typ in the two conversion cycle mode?
I take back my question about the bootloader.
Regards,
Kazu
Hi Logan,
About the way to speed up by using two LTC2986s, how can I get 12ch in 1s since this part's ODR is 164ms typ in the two conversion cycle mode?
I take back my question about the bootloader.
Regards,
Kazu
I installed QuikEval software and downloaded all the latest driver. However, the DC2026 board is not getting recognized.
Thanks,
B
During initial power up, all the status register are initialized to zero. This will then followed by the digital initialization where the command status register will return to 0x80 for about 100ms. Once the initialization process is complete, the command…
Hi,
If you check CN0384, there is a section for Multiple Thermocouple System (page9) wherein you can connect at most 6 thermocouples with respect to the same cold junction using AD7124-8. So in your case you can use 3 AD7124-8 to accommodate the 18 thermocouples…
Hi @dariaa - apologies for the delayed response.
1) Leakage current will affect sensors and filters with high series resistance. My article goes into more details but you may see degraded accuracy with large series resistances at hot - keeping any filter…
Update:
Just to be specific about what pins I’m talking about and how we’re using them I made this list:
LTC2449:
~CS Our designs: Tied to GND / Return
From datasheet: A LOW-to-HIGH transition on CS during the Data Output aborts the data transfer…
Question:
Can I use the sample codes on different microcontrollers?
Answer:
You will need the Linduino sketchbook if you want to keep the LTSPI calls from the generated code. If you do not intend to use a Linduino, replace these with standard SPI calls…
Question:
Can I get sample codes for the LTC298x family?
Answer:
The LTC298x demo software includes the capability to generate a C code. Sample codes for demo boards and examples shown in the datasheet are included in the Linduino sketchbook. Codes…
Question:
I want to design a custom board for the LTC298x family, can you provide a design reference?
Answer:
Please refer to each part’s evaluation board design files. Schematic and layout examples are available on their Product Pages. You may ignore…